Other Parts Discussed in Thread: ADS1274, ADS1278
测量ADS1274的DOUT[5:8],竟然和地是通的,这是怎么回事? 是芯片的问题?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好!
首先ADS1274的DOUT[5:8]是不使用的,通过ADS1274的datasheet,你可以看到对DOUT[8:5]引脚的说明” Internally connected to active circuitry; outputs are driven”. 而其相应的输入引脚AINP[5:8]和AINN[5:8]都是处于悬空状态的,ADS1274在使用的过程中DOUT[8:5]也是可以直接悬空的,具体可以参考ADS1274EVM上的电路设计。DOUT[5:8]与地相通不一定是ADS1274的问题,可能在芯片内部已经将DOUT[5:8]接地,以防止悬空时引入各种干扰。
谢谢~