This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于ADS1274的TDM输出问题?

今天调试中发现一个问题,1274在用DRDY+TDM输出模式下,读到的第一个字节是无效的!

配置是4通道,在DRDY下降沿产生后,等待5us(采样率25K,即间隔40us)给出SPI的SCLK,如果连续采集发现一共有13个有效读数的字节,而不是12个。多次试验后,可以发现最后一个字节的最后一位有的读到的1,后面全部是0,因而可以排除其他可能,确实是采到了13个字节。如果把第一个字节去掉,得到的值和所给波形就吻合了。

在手册中貌似没有发现这一条,不知是不是我这边其他的问题,望能给出明确答案!