This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS422x 告诉采集的数据转换问题

Other Parts Discussed in Thread: ADS4225

各位

       现在有个案子用到ADS4225告诉采集芯片,采集酸速率100M。 按照资料和参考设计,需要在查分输入端接入VCM(common-mode电压)来进行整体偏置,VCM偏置电压为0.95V,这样就是差分输入信号,整体抬高在0.95V电平上下。在这样的设计输入下,从ADS采集到的数据有个很奇怪的现象。

1. 没有输入信号时,采集信号接近0XFFF, 为满数据值

2.当有正弦信号时,输入高于VCM时,呈现为从0X000开始上升到峰值电平时回落到0X000。

3当有正弦信号时,输入低于VCM时,呈现为从0XFFF开始下降到波谷电平后回升至0XFFF。感觉吧正弦波分成了两段、

4另外这款芯片的基准电压是多少,用于从采样数据到实际采样值得换算的基准电压。

5由于采用VCM为差分输入的共模偏置,那我的采样数据和采样值应该怎么换算呢。