请教以下问题:
1,如图是green led driver的原理图,我的理解是R216左侧的LED_EN信号能控制Q17的Vgs从而控制led的亮灭,但是还没弄清楚通过调节LEDG_PWM的占空比怎么调节led的亮度?
2,测试发现U46的7脚VSENSE处电压稳定为0.8V,从LEDG_PWM出来的pwm波经R217和C272滤波后也基本变为直流,那led光源的阳极(ANODE)和阴极(CATHODE)之间的电压和电流是如何变化达到调节led光源亮度的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请教以下问题:
1,如图是green led driver的原理图,我的理解是R216左侧的LED_EN信号能控制Q17的Vgs从而控制led的亮灭,但是还没弄清楚通过调节LEDG_PWM的占空比怎么调节led的亮度?
2,测试发现U46的7脚VSENSE处电压稳定为0.8V,从LEDG_PWM出来的pwm波经R217和C272滤波后也基本变为直流,那led光源的阳极(ANODE)和阴极(CATHODE)之间的电压和电流是如何变化达到调节led光源亮度的?
@Kevin Shi
上图中的power dowm电路用于放电的话,断电时DMD光机模块也为VOFFSET,VRST和VBIAS的负载,为什么要额外设计放电电路?