准备用DLP3010芯片做曲面投影实验,需要60Hz 720p的外部视频HDMI输入。
查询到DLP3010的评估板有两款产品:
DLP3010EVM-LC
DLPDLCR3010EVM-G2
请问这两款产品的区别是?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
准备用DLP3010芯片做曲面投影实验,需要60Hz 720p的外部视频HDMI输入。
查询到DLP3010的评估板有两款产品:
DLP3010EVM-LC
DLPDLCR3010EVM-G2
请问这两款产品的区别是?
您好!
没有深入了解过3D打印,按我的理解3D打印也是投影一副图案,和显示领域的投影有什么不同呢?
->比如说打印只需要单色的LED(可以通过pattern模式实现),而投影通常是RGB三色。在显示应用中控制器会增加一些TI的算法来使图像显示更加优化,而这在3D打印中是不需要的,还有其他一些不同。
查询到这两款EVM的芯片都是DLP3010,波长、分辨率、帧率等参数完全一样,控制芯片DLPC3478+DLPA2005和DLP3433+DLP3000给开发者带来的使用上的功能差异是什么?
->DLP3010A和DLP3010LC功能是相同的。DLPC3478具有pattern功能,同时提供了对外的同步接口Trigger out、trigger in、patter ready等,在pattern模式下能将显示算法bypass掉,使显示更加准确,而DLPC3433没有。DLPA2005、DLPA3000是电源芯片,可以根据实际的需要选择合适的芯片。
对比了他们的Block Diagram,DLPDLCR3010EVM-G2没有camera trigger接口,如果想使用外部摄像机的图像反馈来进行图形校正,是不是只能选择带有camera trigger接口的DLP3010EVM-LC?
->这取决于您实际需要DLP实现的功能,
DLPC3478能够实现快速投影特定的pattern(1bit@2500,8bit@360Hz),并且能够结合Trigger信号实现高精度的同步,实现高精度的3D 扫描。
如果只是简单的功能,比如定位投影的位置,也可以使用DLPC3433特定的图片。
另外,这两款EVM带有投影图像的梯形校正功能吗?
->支持1D的Keystone,但是需要手动输入矫正角度,没有自动keystone
Best regards