This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPLCR4500EVM 用GUI加载大量图片并按1bit 图像播放如何设置

您好!

      问题描述:我想采用GUI加载约1200张1bit图片,并按指定顺序播放,播放速率希望可以达到4kHz

      目前状态:将1bit图像合并成了24bit图像,并且可以按照指定顺序播放,但是播放最大曝光时间240us, 周期为480us。

      问题:1 如何让每一个1bit的图像播放周期减小到240us,以使得播放频率可以大于4kHz?如果我这样是采用的是External RGB Input Pattern,只能达到2880Hz,那么如何才能配置为Preloaded Pattern呢?

                 2 将1bit图像合成为24bit图像后,约51张24bit图像,烧写过程中到95%左右时,提示报错,是什么原因呢?

                 3  每次播放前,需要一张一张地指定播放顺序,在图片较多时,不是特别方便,是否有其他的方式可以让GUI按24bit图片顺序加载,并按一定的RGB通道顺序1bit-1bit地顺序播放呢?即是否有简便的方式,而非每一张图都需要点击鼠标好几次。

                4 说明文档当中提到vidio模式,也是按1bit的图像进行播放的,是否可以理解为,如果把24bit图像按照顺序做成vidio,最后播放出来,对于1bit图像而言也就是达到2.8kHz以上呢?(这样是属于External RGB Input Pattern吗?)

谢谢

wangxi