Other Parts Discussed in Thread: DLP4500, TPS65145
按照贵司DLP4500的EVM设计原理图,如下图,但是最终生产时,电感并未选择22uH而是10uH,是否对于DLP4500的驱动不会造成太大影响?即在其工作温度范围内仍可正常工作呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
按照贵司DLP4500的EVM设计原理图,如下图,但是最终生产时,电感并未选择22uH而是10uH,是否对于DLP4500的驱动不会造成太大影响?即在其工作温度范围内仍可正常工作呢?
谢谢!
从datasheet上,我看到不同电感下得到的纹波有差异,10uH与22uH,大约是差2倍。这样看来的话,如果接受这个纹波差异,那么就可以使用。不知道我的理解是否正确?
另外,图纸上选择的电感是DTC1608C-223,其电流参数如下图,并且是1MHz下的参数而非TPS65145的工作频率1.6MHz,真的能够符合此处的要求吗?
为何事实上DLP4500对于三个电压耗费很小,只有不到10mA而已,但是在使用TPS65145等进行计算时,却是达到0.96A的开关电流限制呢?
TPS65145并不是专门面向DLP系列芯片的供电芯片,所有datasheet上的计算不没有针对DLP的SPEC来进行计算。你们可以自己根据参数重新计算,纹波部分叠加后需要满足不超过DMD datasheet上规定的最大最小电压。