This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC3479: Run Once指令运行不止一次,连续出图

Part Number: DLPC3479

硬件方案:C3479+C4710+A3005,由FPGA进行控制

控制逻辑:光机3479写入12张图片,FPGA收到外部触发信号后,通过I2C给3479发送Run once命令,3479在投影的同时,通过输出的 Trigger_out 2 信号触发相机进行拍照,相机会进行计数,满12张后进行处理。

问题描述:出现问题时,发送Run once指令给光机,光机 Trigger_out 2 输出的信号不止12个,导致与相机交互异常。

下载12张图片的配置如下图:

正常运行时,抓取波形如下图:

出现异常时,抓取波形如下图:

对比正常情况下与异常情况下发送的I2C指令波形,基本一致: