This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC2G17: Buffer器件的输出延迟与抖动参咨询: SN74LVC2G17

Part Number: SN74LVC2G17


你好,请教Buffer器件的输出延迟与抖动:

我们使用Buffer器件经cable线(长约2m)驱动相机触发,信号为2MHZ duty 20%的方波;

想了解如下规格书中,信号经板上特定Buffer器件(SN74LVC2G17),延迟(tpd)是一个固定值,还是在不同的周期延迟(tpd)在min~max之间波动?

因为我们的应用对触发的时序要求(信号边沿)很关注,如果信号经buffer后,输出信号边沿抖动,对应用影响比较大 ;

可以增加输出驱动,信号输出延迟(or尤其是抖动)比较小的合适器件,请推荐。

感谢~

sn74lvc2g17 tpd.png