Part Number: HD3SS215
Hi, I want to use this switch between a smarc module DP++ and 2 phisical DP++ connectors.
How can I switch the config2 signal from the 2 DP? Is it possible?
Thanks.
Luc Buc.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
This mux is a 2:1 Display Port compatible mux, so it should be able to switch between one module and 2 connectors.
You may need a secondary mux to switch in the config2 signal if you plan on using the 1st mux to switch a full set of display port signals.
Depending on bandwidth requirements of your system, a 6 channel 2:1 mux could be used instead, such as the TS3A27518E. You can find other high speed 2:1 muxes with 5+ channels on our selection guide here!