大家好,我采用的是6678evm中的接法,如下图示,请问为什么晶振不能起振,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
62005里有个smartmux,里面有选项供用户选择是PRI_in,还是SEC_in,或者是AUX_in,你检查一下设置对了没有。另外输出端也有一个mux,可以切换到PRI,SEC,AUX和VCO,你可以试一下从smartmux里选择AUX_in以后,输出mux也选择smartmux,看看有没有输出。另外,62005EVM的User Guide在官网可以找到的,链接如下,你可以对照着你的电路图比对一下。
你好 Decapton
现在晶振能起来了,但是幅度比较小,峰峰值为1.2V,请问AUX的输入的电气要求在那边找?我在数据手册上没看到
我也没找到AUX的电气要求。不过
1. 从手册13页“DIFFERENTIAL INPUT MODE (PRI_REF, SEC_REF)”来看,最大的差分电压在1.3V,目前AUX电压峰峰值在1.2V,我觉得应该够用了。
2. 1.2V峰峰值已经有5.5dBm了。之前我用62005,2dBm进PRI,环路是能锁定的。估计AUX输入有1.2V峰峰值,应该没问题。
3. 47pF的对地电容在25MHz时等效的电阻有136Ω,这是个很大的负载了,为什么在这里加这样一个电容?手册里没有提到这种用法啊。建议去掉,或者改小。
Decapton 你好,我现在的并联电容选择了8.2pf。47pf 电容晶振起不来
个人理解,在那边放一个电容,目的是造一个高频交流地,把晶振的高频噪声滤掉。但是这样做直接后果是对晶振造成一个负载,你可以看一下晶振的数据手册,看看上面对晶振能够驱动的容性负载有没有什么具体的解释。然后再按照我之前的回复,看看1.2Vpp的AUX输入能不能使PLL锁定。