Other Parts Discussed in Thread: TS3V713EL, TS3V712E
各位好,
我用TS3V713做了一个vga2:1切换器,现在有一个问题。就是在芯片没上电时,输入信号的两个同步是正常的,5V电平,负脉冲。但是当芯片上电后这两个输入同步信号就变成了3V左右,脉冲极性和频率宽度不变,也就是说只是电平被拉低了。这时从输出口测试,RGB三个颜色信号都能被捕获到,虽然不能确定正确,但是从示波器看应该差不多。但是两个同步信号一个都没有。
我看手册这两个信号是用那个5V供电的,我确定接上了。电路也很简单。几个电源各有一个0.1uf去耦电容。视频信号直接连接到vga连接器。
请问这是什么原因?是否可能是5V接触不好导致的?我换了两个芯片,都是这个现象。
另外5V电源品质要求是否严格?我用的开关转换器,有几十个毫伏的纹波。
谢谢。