Other Parts Discussed in Thread: SN65HVD101
大家好,在使用SN65HVD101的时候,如果使用片外5V给芯片供电,VCC_OUT该怎么处理呢?
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
VCC_OUT是HVD101内部regulator的输出引脚,可用来给自身或者其他设备进行供电,输出3.3V还是5V取决于Vcc_SET的接法。
如果不使用VCC_OUT的话,可以直接悬空,或者本身给regulator的供电电压L+也不需要外部供电了,直接不使用内部regulator了。
或者建议使用其他不集成regulator的CAN tranceiver。