Other Parts Discussed in Thread: SN74LV4T125, LSF0101
之前在一个项目中用到了电平转换芯片ALVC164245,芯片耐温为125度,通过加温实验后发现当工作温度为100度时,+3.3V供电电流会出现较大幅度增加,从室温的1mA增加到19mA,此端主要与FPGA连接,FPGA端电流是保持稳定的。+5V端电流增长不明显。对+3.3V电流增长不清楚。
为了减小电流消耗,准备用SN74LV4T125 来替换ALVC164245,因为该芯片+5V单电源供电即可,如果芯片工作温度依旧为100度,请问使用该芯片替代可以吗,还有芯片LSF0101,使用该芯片后电流会有很大变化吗?望大神给予解答!
谢谢!!!