Other Parts Discussed in Thread: SN74HC132, SN74HC32
SN74HC132 可以输出驱动电压为5v的信号,那么这个信号如果连接到CPLD的io上,就相当于要求这个CPLD I/O 能够承受5v电压。
为什么推荐的Vcc是5V,3.3v 应该是常用的呀?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
VCC范围是2~6V,用在3.3V也没问题的哈。并且后面的一些电气参数的测试条件也不只是局限于5V。
推荐5V,是因为5V供电的话,其性能最佳。
如果需要推荐3.3V的话,可以选择其他器件,TI的每款器件基本上是适用于不同方面的应用,满足不同客户需求。
谢谢。但是如果用3.3v,输出驱动应该就是3.3v了吧。
另外特性中提到 ±4-mA Output Drive at 5 V,是指Vcc在5v情况下,输出驱动电压是5v,输出的电流范围是+-4mA?
请问Vcc是5v时候,C1 C2是同一个单端信号,高电平是5v,经过与非处理后,出来的OUTC信号高电平怎么是4V。但是给A1A2一个TTL 3.3v,出来的信号高电平却是5V。
可以看下Voh和Vol的测试条件,是在Ioh和Iol一定的条件下测试的,+-4mA指的SN74HC32的source/sink电流,也代表了SN74HC32的驱动能力。Henry W 说:谢谢。但是如果用3.3v,输出驱动应该就是3.3v了吧。
另外特性中提到 ±4-mA Output Drive at 5 V,是指Vcc在5v情况下,输出驱动电压是5v,输出的电流范围是+-4mA?