This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP28335与DA转换芯片TLV5610的引脚对接时钟问题



第一次使用这款DA数据转换芯片,在看芯片手册的过程中有一些不明白的。

1.引脚编号为4的FS的作用是Frame sync input,表示帧同步输入。但是在DSP工作模式下,要求FS必须在第16个时钟下降沿前回到高电平,这一点如何能保证呢?另外,还要求FS在变成低电平之前必须要有SCLK的下降沿并且两者至少间隔5ns以上,这个又该如何保证呢?在接线的时候,FS该接到dsp的哪个引脚呢?

2.TLV5610的数据长度是16位,其中前4位为地址位。当我通过这4位进入控制寄存器进行设置的时候,只需要继续写一个设置命令就可以了吗?之后再继续写,会不会被认为继续是对控制寄存器的继续设置呢?

3.我使用的是浮点型DSP28335,那么在将程序中的变量送入到SPI的SIMO引脚进行da转换的时候,该浮点型数据如何能对应到0X000~0XFFF之间呢?