Other Parts Discussed in Thread: ISO3088
请问ISO3088在应用的时候,总线A\B如果采用上下拉电阻,请问是A上拉、B下拉;还是B上拉、A下拉。其上下拉电阻取多大适合?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ISO3088
请问ISO3088在应用的时候,总线A\B如果采用上下拉电阻,请问是A上拉、B下拉;还是B上拉、A下拉。其上下拉电阻取多大适合?
Use 1-kΩ to 10-kΩ pullup and pulldown resistors for enable lines to limit noise currents in these lines during transient events.
这里的上下拉电阻是failsafe bias 电阻。一般是A上拉,B下拉,上下拉电阻取值相同即可。
datasheet中给出的经验值为1K到10K,其实是可以计算的,在这篇design guide中有详细介绍,可参考:http://www.ti.com/lit/an/slla272c/slla272c.pdf
还有一个问题,ISO3088靠近MCU侧的R内部有没有做上拉,设计应用时是不是应该在外部加一个上拉?用来确保
异步通信从一个低电平握手开始。
您好!在使用ISO3088过程中有个问题一直想不通(之前的485设备可以正常收发、新的485设备不可正常收发--返回数据量比之前的设备大),想请教下。具体现象如下所述
a、我们主要是应用在MCU发送命令读取设备测试数据(设备收到该命令后会返回60个字节)。
b、通过示波器监测MCU端的RX和TX,发现TX有数据发出、而RX未接收到数据。
c、当将usb转485串口工具接到电脑上的串口调试助手后,此时RX可以正常收到数据。
d、不接入串口工具,仅通过在A、B线上增加上下拉电阻,此时RX未接收到任何数据。