如图所示,使用了一个CWX813-20MHz的CMOS时钟,和一个7B-10.000MEEQ时钟。
为何做这样的设计?
我正在设计一个扫频仪,是否可以使用单一晶振为LMX2571提供时钟?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如图所示,使用了一个CWX813-20MHz的CMOS时钟,和一个7B-10.000MEEQ时钟。
为何做这样的设计?
我正在设计一个扫频仪,是否可以使用单一晶振为LMX2571提供时钟?
这里是使用了两个外部时钟源产生差分时钟OSCin和OSCin*给LMX2571做参考时钟。
如果您想使用单端晶振也可以,没问题。
我一直没能理解其中的C3/4,R3/4。希望能为我解答。
默认选择C1C2R2就可以了。可以满足90%的情况
如果是在性能不可以时,引入C3C4