您好,我在使用LMK04616这个芯片过程中,只配置了OSCIN、CLKIN、PLL1_RDIV、PLL1_NDIV、PLL2_RDIV、PLL2_NDIV以及OUTCH的寄存器,更改PLL2的RDIV以及NDIV寄存器,通道输出的频率是发生了变化,但根据频谱仪以及读去STATUS的数据,发现该频率没有锁住。想请问我还需要配置哪些寄存器才能将PLL锁住,以及是否有辅助寄存器配置的工具,可以帮助我完成对该芯片的控制?期待您的回答,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,我在使用LMK04616这个芯片过程中,只配置了OSCIN、CLKIN、PLL1_RDIV、PLL1_NDIV、PLL2_RDIV、PLL2_NDIV以及OUTCH的寄存器,更改PLL2的RDIV以及NDIV寄存器,通道输出的频率是发生了变化,但根据频谱仪以及读去STATUS的数据,发现该频率没有锁住。想请问我还需要配置哪些寄存器才能将PLL锁住,以及是否有辅助寄存器配置的工具,可以帮助我完成对该芯片的控制?期待您的回答,谢谢。
你下载一个TICS PRO,免费软件,然后在LMK04616里面按照你的设置配置好,它会生成寄存器文件的
恩,可能还是寄存器没配置 好, 安装TICSPro,参考LMK04616EVM user's guide中使用TICSpro的步骤。
http://www.ti.com/tool/ticspro-sw
在使用过程中如果还出现什么问题,可随时讨论。