如果使用TUSB2046不外接EEPROM,EECLK和SUSPND NC,EEDATA/GANGED 和EXTMEM拉高,将4个VRCUR全部上拉以及4个PWRON全部NC这个是否可行?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如果使用TUSB2046不外接EEPROM,EECLK和SUSPND NC,EEDATA/GANGED 和EXTMEM拉高,将4个VRCUR全部上拉以及4个PWRON全部NC这个是否可行?
不接EEPROM,EXTMEM拉高disable EEPROM, EECLK和SUSPND为输出接口,悬空即可。
EEDATA/GANGED这个引脚用作GANGED功能 ,高电平或低电平都没问题,If GANGED is high, all PWRON outputs switch together and if any OVRCUR is activated, all ports transition to the power-off state.
If GANGED is low, the PWRON outputs and OVRCUR inputs operate on a per-port basis.
如果OVRCUR和PWRON不和外部Power IC连接的话,可以直接NC。
另外,TUSB2046已经停产,建议使用TUSB2046B来替代。 并且也提供了自供电和总线供电的两种电路图,可直接参考。