Other Parts Discussed in Thread: TXV0108, TXB0108
请问下,我的设计中需要将FPGA的1.8V和1.5V电平信号传输到单片机3.3V的,信号包括SPI、UART、高低电平控制信号、LED指示灯的负端等其他信号,找到TXV0108这个芯片,有几个疑问:
1:TXB0108是自动判断信号传输方向的,那在同一片芯片里面,是不是每个口都是相对独立的,例如我要传输SPI,3.3V单片机的MOSI从B口到A口变成1.8V,那同时可不可以1.8V的MISO信号从A口到B口变成3.3V,同时其他口也是A到B或者B到A同时在工作,这样工作可以吗,还是说同一时间全部口只能同一个方向?
2:TXB的驱动能力不强,那我用作变换电平后的LED指示灯的负端(0V)是否可以呢,电流小于10mA
3:可否讲解下TXB0108变换电平的原理呢?