Other Parts Discussed in Thread: ISO1541, ISO1540
我今天做实验用ISO1540 和ISO1541 做信号隔离。我使用信号发生器发出频率100Khz的波形给芯片的SCL1 然后我用示波器在SCL2测量波形,但是测量不到。然后我调小频率到几百hz。SCL2也是没有波形。 我的电路就是VCC1和VCC2 GND1 GND2 分别接电源。然后在SCL1 和SCL2 加了一个1.5K上拉电阻。 请解答一下
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
频率没问题,支持的I2C的速率,最大为1MHz。另外上拉1.5Kohm也没问题。
根据您的描述,电路是没问题的,VCC1和VCC2也没超过供电电压最大值吧? 先检查下输出引脚是否有脱焊现象呢。
您是指的电源的去耦电容吗? 那里的电容是滤除噪音的, 跟SCLK没有输出应该关系不大。