Other Parts Discussed in Thread: LMK04828BEVM, CODELOADER, USB2ANY, LMK04828
发现用LMK04828BEVM开发板可以在线下载配置文件但是无法固化程序,那请问我们自己设计LMK04828B的板卡可以固化程序吗?怎么在codeloader软件操作呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LMK04828BEVM, CODELOADER, USB2ANY, LMK04828
发现用LMK04828BEVM开发板可以在线下载配置文件但是无法固化程序,那请问我们自己设计LMK04828B的板卡可以固化程序吗?怎么在codeloader软件操作呢?
好的,谢谢您的回答,我顺便想再问一下,因为这个系列的芯片都只有SPI通信接口,为什么电脑上安装的Codeloader软件并通过USB2ANY下载器将配置文件下载到芯片中不能固化呢,这一过程按理说也是对芯片的寄存器进行的写操作,也同样能够起到固化作用才对。这和您说的FPGA或MCU通过SPI接口将寄存器配置写到芯片内部难道不是类似一样的方法吗?只是传输途径不同而已。麻烦您再进一步解释一下这两种方式的区别在哪里,太感谢了。如果必须通过FPGA或MCU进行寄存器写操作才可以固化,那么在实际设计产品时就不用Codeloader软件和USB2ANY下载器了对吗?
你说的固化是什么意思?
我理解的是固化就是把参数写入到LMK04828芯片内部。芯片掉电,再上电后不需要外部配置,就可以直接工作。
LMK04828芯片内部没有EEPROM,不能固化参数。芯片掉电后,所有的配置信息就丢失了。所以需要外部的MCU或者FPGA进行配置。
我说的固化跟您上面说的是同一个意思,那就是说codeloader软件和USB2ANY下载器只能在前期评估板上在线下载使用,后期做产品的话这两样工具用不到;如果做产品的话,为了保证脱机使用,而LMK04828本身又没有非易失性存储器电路,只能将控制其内部各种寄存器的程序写到MCU或FPGA中,板子每次上电MCU或FPGA的非易失存储器加载程序后,再通过SPI接口来输入LMK04828所需的寄存器配置数据,来达到时钟输出的目的。我的理解对吗?
是的。就是您说的这个意思。所以不能把配置固化到芯片里面
如果对性能要求不是特别高,可以看看62005.他可以固化程序