Other Parts Discussed in Thread: LMK04828BEVM, CODELOADER
各位技术大牛好,我是初学TI这种高速时钟去抖合成器,选用的型号是LMK04828B,使用配套的评估板LMK04828BEVM进行前期的开发测试,第一次使用准备输出500MHz的时钟,通过更改codeloader软件的PLL1、PLL2和CLKOUT这三个选项卡的参数,在线下载配置文件后输出正常,Status_LD2的指示灯点亮。更改了一些其他配置(比如在codeloader软件上点了read all以及option选项卡的一些选项),不知什么情况,再下载配置文件后,时钟信号虽然有输出,但一直输出480MHz左右,总是偏离正常值几十兆赫兹,且Status_LD2的指示灯也不亮了,之后不管怎么修改coadloader软件配置都不管用,请问这种情况如何解决,试了一周了,没有有效的办法,请专业人员帮忙支个招,万分感谢!