Other Parts Discussed in Thread: DS25BR204
最近一项目中有用到DS25BR204这颗芯片,作为一输入二输出使用。目前方案评审已经完成了,准备开始硬件设计。
但是测试发现,输入给DS25BR204的LVDS信号Jitter抖动比较大,输入给DS25BR204的LVDS信号测试具体如下
1:输入信号的抖动Tj(1e-12)约为400ps~450ps之间,
2:输入的信号速率约为1.58Gbps.
在DS25BR204这颗芯片上并没有找到关于对输入信号Jitter的要求,并且因为DS25BR204在我们这个方案中处于前端比较重要的位置,对于上面我提到的这种输入信号,DS25BR204是否能够有效处理???
PS:
输入给DS25BR204的信号是从别人的板卡上来的,我们这边暂时没法优化。