Other Parts Discussed in Thread: DS90UB934-Q1EVM
Hi TI Team
我们在使用DS90UB933和UB934设计时,使用SONY的IMX019的传感器,933和934的寄存器采用初始配置,没有做更改,目前遇到如下问题。
1)当传感器这边IMX019输出74MHZ频率时,10bit, 933和934能正常传输,能正常显示图像。而934的输出时钟频率翻倍了,达到148Mhz,这是否正常?
2)当图像传感器输出99Mhz频率时,10bit, 933和934不能正常传输,934输出的图像是不连续的,间断的,不完整,这有什么办法解决?因为Sony的技术支持表示有其他客户使用933/934正常传输了99Mhz的信号。这里是否需要配置一些寄存器?,哪几个寄存器比较关键? 我们的产品设计需要99Mhz的频率。
3)我们使用过913/914,933/934设计过多款产品,但是均没有配置寄存器能工作。后期我们还在正在开发953/954的产品,针对寄存器配置这块是否有详细的配置说明,如先后顺序,不同模式下的配置方式等等。这对于我们开发产品会有很大帮助。我们前期用到Maxin的同类产品,均提供了这方面的详细说明。
所以请share寄存器的配置说明,langmings@126.com