This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助:DP83848K 自适应灯灭掉



现象描述:设备进行长时间拷机后(网线插着,以太网100M正常工作)发现个别设备,自适应灯会灭掉,但是交换机上的网速速率匹配显示是100M,并且网络通信正常,但是如果100M切换为10M的话,设备速率会匹配不上,导致网络失联。

  • 您是指的LED_link和LED_speed这两个LED吗? 这两个LED的on, off以及blink的情况可以参考Table 6-2. LED Mode Select for DP83848x的介绍。
    另外,对于10Mbps的速率来说,link正常的话,需要:A 10 Mb/s Link is established as a result of the reception of at least seven
    consecutive normal Link Pulses or the reception of a valid 10BASE-T packet. This will cause the assertion of LED_LINK 。
  • 您是指的LED_link和LED_speed这两个LED吗? 这两个LED的on, off以及blink的情况可以参考Table 6-2. LED Mode Select for DP83848x的介绍。
    另外,对于10Mbps的速率来说,link正常的话,需要:A 10 Mb/s Link is established as a result of the reception of at least seven
    consecutive normal Link Pulses or the reception of a valid 10BASE-T packet. This will cause the assertion of LED_LINK 。
  • 是的  ,刚开始工作的时候这两个灯都是正常的,但是拷机拷一段时间后,有部分设备的LED_SPEED灯会灭掉,但是网络连接正常,LINK灯也正常,但是灭掉后我如果交换机那边的网络速率有100M切换成10M , 网络就会失联。