This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH0001的Rref的问题

Other Parts Discussed in Thread: LMH0001

我在使用lmh0001时,注意到datasheet上提到可以通过修改Rref的值来控制输出电压的摆幅,我现在需要在驱动能力和功耗间取得一个平衡,但datasheet上仅仅给出了Rref为750R和590R情况下的输出电压的摆幅,请问关于Rref的值与输出电压摆幅是否有一个具体的曲线关系?这样我可以根据需要的摆幅来确定具体的Rref的值。另外我在尝试自己改变Rref的值时遇到了困难,手工焊接和拆卸这个电阻似乎非常容易造成芯片工作的不稳定。

  • 您好,
    SMPTE 259M / 344M SDI接口信号应该都有信号技术标准吧,不能随便调吧 我建议按照数据手册上的参数来设计电路。
  • 您好:

    datasheet上关于Rref的描述是这样的:

    Output driver level control. Connect a resistor to VCC to set output voltage swing.

    Output level is controlled by the value of the RREF resistor connected between
    the RREF pin and VCC.

    我的理解是可以通过改变Rref的值来控制输出电压摆幅

  • 是的,Rref上拉电阻阻值可以控制输出swing,但是没有线性关系曲线可以参考,典型应用就是上拉75ohm输出800mVpp swing,另外,如果您需要输出降低swing符合MADI标准的话,建议将Ref上拉电阻为1.1Kohm,这样输出swing为400mVpp。