Other Parts Discussed in Thread: ISO1050
一批板子中,出现了大量的通讯故障问题,发现是ISO1050坏了,CANH和CANL脚之间电阻由正常的5.2k左右变为无穷大,VCC2-GND2之间电阻变得很小,拉低了隔离电源。损坏原因不明,器件的共模耐压±12V,那么我用PESD1CAN(24V)接在CANH(或CANL)到GND2之间,是不是没有起到防护作用?手册上CANH或CANL有-27V到40V的耐压又是指什么?最重要的是损坏原因是什么?怎么更改?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ISO1050
一批板子中,出现了大量的通讯故障问题,发现是ISO1050坏了,CANH和CANL脚之间电阻由正常的5.2k左右变为无穷大,VCC2-GND2之间电阻变得很小,拉低了隔离电源。损坏原因不明,器件的共模耐压±12V,那么我用PESD1CAN(24V)接在CANH(或CANL)到GND2之间,是不是没有起到防护作用?手册上CANH或CANL有-27V到40V的耐压又是指什么?最重要的是损坏原因是什么?怎么更改?
1、坏机上的PESD1CAN拆下来测试是好的,30V的时候电流有5mA,与手册一致。
2、CANH和CAN到GND2之间的阻抗有些是正常的无穷大,有些是已经到了1k以下;而CANH和CANL之间我也测了,正常应为52k左右,而故障的样机有的是无穷大,有的是其他阻值,都是不正常的。
3、拆掉ISO1050芯片后,电源电压就正常了。
4、另外,出问题的样机全部集中在同一批,同一时间。
由上可知,的确是ISO1050出问题,现在在推测它损坏的原因:1、周边防护器件没有到位或者是没有起到作用;2、买到水货;3、现场工人操作不当。这样推断是否合理?