Other Parts Discussed in Thread: TXS0108E, SN74AVC32T245, SN74CBTD16211
目前的设计中希望将PCI接口和FPGA相连,FPGA侧电平为1.8V,PCI接口侧为3.3V,PCI频率为33.3M,目前想采用的连接方式是FPGA I/O - TXS0108EPWR A口 - TXS0108EPWR B口 - 电阻 -PCI接口这样连接,VCCA接1.8,VCCB接3.3或5V(主机侧PCI电平取决于主机,需要兼容3.3或5)
有几个问题,(1)这款芯片的速率是否可以支持PCI的应用,手册上写最大线速率是60M,但是很不确定是否可以应用于PCI? (2)A口和FPGA信号是否可以直接相连(一部分信号是FPGA输入,一部分是FPGA输出) (3)B口和PCI接口之间是否需要电阻,如果需要的话大概取多大的阻值?(4)看手册上似乎芯片内部有上拉,所以A口和B口两边的信号都不需要上拉吗?