This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0104E电平转换异常



您好,我按照数据手册提供的典型应用的电路图做实验,从B端口输入Vpp为3.3V的交流信号,观测A端口的输出情况。当输入信号为700Hz时,A端口的输出为2.8V,已经比VCCA(1.8V)高了!而且,随着输入信号的频率升高,A端口输出信号的峰峰值会有所下降,在输入信号为2MHz时,A端口输出信号的峰峰值为1.8V左右。我对此我有以下几个问题:

1、为什么在频率较低时,portA输出的信号幅值要比VCCA还大

2、输出信号的幅值随输入信号的频率变化的原因是什么