This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用DS92LV2421作为信号的传输中介,传输的信号是12.5M。

Other Parts Discussed in Thread: DS92LV2421, DS92LV2422

DS92LV2421/22-EVK评估板测试过程

目的:利用DS92LV2421/22传输信号:

输入信号类型:时钟信号1-频率12.5MHZ,数据1(该时钟信号为双边沿(上升沿/下降沿)传输数据)

             时钟信号2-频率7MHZ,数据2(该时钟信号为下降沿采样)

             控制信号

测试过程:

  1. TX板拨码开关设置:RFB=0;PDB=1;CFG0=0;CFG1=0;VODSEL=1;RESO=0
  2. RX板拨码开关设置:BISTEN=0;RES0=0;PDB=1
  3. 外部信号源发生器设置为72MHZ,连接TX板的PCLK;RX板的PCLK输出未连接
  4. 待传输信号连接TX板的R7;G0-G7,B0-B6;未完全占用RGB接口
  5. 输出信号经过RX的对应连接器连接到灯板
  6. 该操作模式下,可完成信号传输 

 问题:需要传输的时钟信号为12.5MHZ,对应的数据有多组,时钟需要双边沿采样;另外一个时钟7M,对应数据多组,时钟需要单边沿采样;该12.5MHZ的时钟能否作为采样时钟,连接PCLK,经DS92L2421的倍频后,采集所有的数据及另外一个时钟;然后经DS92LV2422解串器的分频后,得到原来的信号;