This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDS181 在PIN Strap 模式下无输出

Other Parts Discussed in Thread: TMDS181, TMDS171

使用TMDS181RGZT和TPD12S016RKTR搭建FPGA与显示器的HDMI信号通道(FPGA为发送端,显示器机为接收端),
FPGA中HDMI接口的DDC和HPD等信号电平为2.5V,因此TPD12S016RKTR电平转换芯片使用2.5V供电。
目前问题是:FPGA提供5V给显示器,显示器发送出HPD信号给FPGA,FPGA机通过I2C读到显示器的相关信息,同时发出HMDI时钟信号到retimer,但是
retimer芯片没有输出HMDI信号给显示器。

硬件配置:

1、pin1 SWAP/POL 悬空

2、pin10 I2C EN 64.9k下拉到GND

3、pin17 SIG_EN 64.9k上拉到3.3V (已做过下下验证,无效果)

4、pin21/pin27 EQ_SEL/A0和A1 悬空(已做过上下拉验证,无效果HDMI_output_card_0618-c.pdf

5、PIN 20 PRE_SEL 悬空

6、PIN TX_TERM_CTL 悬空

疑问:

1、目前的硬件配置有什么问题?

2、如何验证retimer芯片的状态,比如standby ,normal work?

3、有输入,没有输出的问题如何进一步分析?