This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX1209+ADS1118实现是否适合用在4路热电偶分时复用测温环境?

Other Parts Discussed in Thread: ADS1118, TMUX1209, MUX507

近期在设计一款多路复用的热电偶测温模块,通过查询手册发现TMUX1209的典型导通阻值较小,因此想采用这款复用器作为信号切换,分时选择将四路中的一路接通到ADS1118作为输入信号,进行热电偶温度的测量,不知这样的选型和搭配有没有问题?谢谢

  • 您好, ADS1118 输入前端已经包含有多路选择器MUX.通过Config Register 的bit[14:12]配置来选择哪一路导通呢. 所以无需再外加开关器件来进行选择.
    www.ti.com.cn/.../ads1118.pdf
  • ADS1118目前只支持2路差分信号的切换,我这边需求的话,共需要接入8路热电偶,因此想搭配两片TMUX1209来实现差分信号的切换,这样的话,同一个时刻ADS1118可以采样两个差分通道,通过四个周期,就可以完成8路差分通道的采样,不知这样的场合TMUX1209是否可胜任,谢谢!
  • 您好,两片TMUX1209的话进行切换理论上 也没什么问题,需要 考虑两片开关器件通道与通道之间信号的Skew.
    可以考虑一片差分信号8:1的开关器件, 我个人认为在设计上更方便一些, 我看了下MUX507这款可以作为8通道差分信号8选1的切换, 并且也可以用于热电偶切换的应用, 就是不知电压是否满足您的要求? 因为相对于TMUX1209来说, TMUX1209 可以1.8V,并且集成输入失效保护, 导通电阻也更低一些的特点.
  • 好的,非常感谢,之前选择TMUX1209主要还是考虑到接通电阻比较低,这样对热电偶信号影响相对较小,我在看一下您的推荐,谢谢