Other Parts Discussed in Thread: DS92LV2422, DS92LV2421
想用DS90UB925Q与DS90UB926Q把LVTTL视频信号通过STP长距离传输,并从接受端端回传简单的诊断信号。
由于不能提供I2C协议接口,想把UART的TX,RX数据通过DS90UB925Q/DS90UB926Q的GPIO接口发送与接收。如果仅仅靠一些引脚置高,低电平是否可以正确配置实现基本功能?包括传输显示数据,回传UART数据。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
想用DS90UB925Q与DS90UB926Q把LVTTL视频信号通过STP长距离传输,并从接受端端回传简单的诊断信号。
由于不能提供I2C协议接口,想把UART的TX,RX数据通过DS90UB925Q/DS90UB926Q的GPIO接口发送与接收。如果仅仅靠一些引脚置高,低电平是否可以正确配置实现基本功能?包括传输显示数据,回传UART数据。
您好,不使用I2C的话,是无法实现主机和remote Des/Ses以及remote slave(camera或sensor)之间的通信的。
那也就无法实现传输显示数据以及数据回传功能。
您这里提到不能提供I2C协议接口,是因为主机没有I2C接口,只有串口UART是吗?
您好,我想使用带有I2C接口的主机是使用FPD link产品的硬性要求,除了 I2C可能没有别的办法来实现这种远程通信。
请问这类SERDES芯片的PCLK或TCLK是如何确定的, 我的理解是要比输入并行数据的最高频率要高, 低于SER芯片所要求的最高频率, 还有其他要求吗?
您好,PCLK是由视频源的分辨率决定的,比如视频源的分辨率为1080p@60hz的,那么就要求PCLK的频率至少大于148.5Mhz。所以要看serdes是否支持这么大的频率。