This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83869HM: 使用DP83869HM制作的zynq7020 FMC板卡无法使用

Part Number: DP83869HM
Other Parts Discussed in Thread: DP83869EVM

您好,谢谢您百忙之中回答我的问题。

我使用的是 DP83869HM芯片制作zynq7020开发板所用FMC板卡,作为外置PHY芯片来使用。设计中,我参考了DP83869EVM中的原理图绘制,仅将其电源改为FMC3.3V供电,其余无大幅度修改。

现阶段问题: 我给与DP83869HM的 IO电压为 3.3V,测量其RX_D,TX_D的电压为1.2V左右,然而,经过HX5008NL变压器后,其电压几乎不可测得,RJ45网口无法使用。

考虑原因:1、经查阅发现使用RJ45为TS公司制作,官方说明不支持千兆,之前与TI技术人员沟通,其表明可以支持千兆,具体情况为知,现阶段无法使用~。

2、zynq7020使用得是petalinux2019的系统,考虑DP83869驱动未安装。

问题:1、如何确定是否使用了 DP83869 PHY芯片,其是否正常工作?

2、如何在petalinux 2019.1 中安装DP83869驱动(在搭建的系统的 .../tmp/.../drivers/net/phy/...中发现有TI公司提供PHY芯片的大部分驱动,包含DP83867,不含有DP83869,考虑为版本问题,尝试在其中添加,编译后仍不能使用)

谢谢您的回答,希望你能解决我的问题。