This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB4041I-Q1: 关于TPS4041的第9脚PWRCTL_POL,高电平有效还是低电平有效的说法,datasheet和评估板使用手册的说法不一致。

Part Number: TUSB4041I-Q1
Other Parts Discussed in Thread: TPS2553-Q1

我准备在电路中使用TPS4041I,搭配TPS2553-Q1,发现TPS4041I-Q1的datasheet和其用户指南(SLLU227 A)中,二者关于芯片第9脚(PWRCTL_POL)的说法是不一致的。如图:

datasheet第7页是这样说的:

上拉=PWRCTL高有效。

SLLU227 A第6页是这样说的:

上拉=PWRCTL低有效。

是我的理解有问题吗?谢谢解答!

  • 您好,

    感谢您的反馈,您的理解没有错,是SLLU227这个文件中描述错了,应该是If the switch is set to the ON position, the terminal is pulled down and the port power control polarity changes to active low.我们后续会修正它。

    请按照 datasheet 中的描述配置电路。