用TXS0104E做双向IO缓冲,输出3.3转5V用示波器判断是没有问题;输入的信号是光电编码信号,高电平5V,转3.3V ,输出电平用示波器测量波形不对。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
用TXS0104E做双向IO缓冲,输出3.3转5V用示波器判断是没有问题;输入的信号是光电编码信号,高电平5V,转3.3V ,输出电平用示波器测量波形不对。
1. 注意:1.65 V to 3.6 V on A port and 2.3 V to 5.5 V on B port (VCCA ≤ VCCB)
2. 请给出不对的波形。