This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCA9306: PCA9306使用时VREF1和VREF2为什么在内部用通过mos接在一起

Part Number: PCA9306

学习使用PCA9306时,比较奇怪的是VREF1和VREF2为什么要通过mos接在一起,主要目的是什么?

VERF1和VREF2作用是做什么的?

EN如果接VREF1的话,就不能使用了吗?

实验中还发现,将1.8V的两个上拉电阻从4.7K调整到100k,波形影响不大,是不是因为PCA9306的输入电容比较小,是PF级的,推荐这样使用吗?

上图是我们常规的用mos管搭接的I2C电平转换,9306相对于这种应用的优势在什么地方?

  • 您好,

    PCA9306的工作原理与 LSF系列电平转换芯片工作原理是一样的,具体请查看下面视频,视频中内容可以解答您上述疑问,每个视频也就两三分钟:

    https://training.ti.com/tlm-lsf-bias?context=1134826-1139264-1134790

    关于I2C上拉电阻的选择,PCA9306手册中也提到slva689文档,其中说明了上拉电阻最大值和最小值的计算方法:

    https://www.ti.com/lit/an/slva689/slva689.pdf

    是的,上拉电阻的最大值由I2C总线的总电容决定,它们组成的RC时间常数决定了I2C数字波形的上升沿;如果调整到100k,波形影响不大,当然可以使用;

    上图是我们常规的用mos管搭接的I2C电平转换,9306相对于这种应用的优势在什么地方?

    PCA9306优点在于可以实现多种电平转换,可以减少BOM物料种类;而mos管搭接的I2C电平转换,由于两端电平不一样,需选用不同VGS的MOS管,且MOS管的VGS一般比较大,不能实现压差较小的电平转换。