Other Parts Discussed in Thread: CDCE913, CDCE925
1)我接入的是4MHz的有源晶振,固定频率.应该怎么接.直接接在1号引脚上吗?
2)输出信号用于USB Full Speed通信(12MHz),以太网同步信号(25MHz),MCU主时钟(200MHz),低功耗MCU时钟(30MHz)可以吗?如果不可以,求推荐可以申请样片可用,而且购买不贵的.
3)我的MCU,支持1.8V和3.3V有源晶振输入,这个应该合适吧,我看文档说是1.8V,150ppm会不会导致同步信号提取各种问题呢?
4)我还没此芯片,我只是学生,想申请能批准2片吗?以前都是我队友申请的,现在他出去玩了.
5)输入晶振频偏有多少要求呢?时钟改变时间是多少.输出部分需要接的电容允许范围是多少.