您好,请问947如何配置使用单link,并且使用通道1和解串器948通信,一直无法读到948寄存器的信息,硬件方面只能用通道1,947这边寄存器该怎么配置啊
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,请问947如何配置使用单link,并且使用通道1和解串器948通信,一直无法读到948寄存器的信息,硬件方面只能用通道1,947这边寄存器该怎么配置啊
您好,DUAL_CTL1寄存器的FORCE_DUAL和FORCE_LINK是怎么配置的?
如果FORCE_LINK 配置为自动检测单link还是双link的话,那么如果硬件是单link的连接,那么FORCE_dual这里应该就是自动配置为单link还是双link。
所以我想看下您的这个寄存器是怎么配置的?
补充下,DUAL_CTL1的寄存器是0x5B,0x5B的值您这边配置的是什么? single link的配置基本上就这一个寄存器。
您好,我这边使用通道0调通了,只需要用到一对差分对,之前我用通道1就一直不行,好像是硬件配置上的问题,改用差分对0就成功访问到解串器,但是我通过寄存器手册配置0x5b为0x21或22或20才成功,双link23推视频信号就失败,这个单双link很奇怪,只用一对差分信号是不是只能用单link,因为差分对1有一个引脚给了12v电压唤醒产品,设置双link推视频信号就好像不行,947推948