This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH0303: link down issue

Part Number: LMH0303
Other Parts Discussed in Thread: LMH0344, , LMH0302, LMH0346

We use LMH0303 + LMH0344 at customer side which links down with 2m cable.

What will be the problem?

What's the difference betwwn LMH0302 and LMH0303? Why the typicall reference circuit uses a re-clock with LMH0303? While there isn't a re-clock for LMH0302?

  • Hello,. The LMH0303 integrated Cable Detect on Output, LMH0302 hasn't the cable detection function.

    Do you mean that if you use LMH0302+LMH0344 could link while LMH0303+LMH0344 couldn't link? 

    We use LMH0303 + LMH0344 at customer side which links down with 2m cable.

    What will be the problem?

    How do you judge the link is down? What is the output level of Fault Pin?

  • No, I'm not sure if LMH0302+LMH0344 will work.

    It links down because the Video Analyzer doesn't get signal (3G-SDI checkfield). While when it is changed to a competitor's product with CDR (LMH0346) inside, it works well.

    I'm not sure what cable driver & cable equalizer the competitor uses. There is only 2 meters + 2 meters coaxial cable in the test setup.

  • 您好,我们还是用中文沟通吧。

    LMH0303是cable 驱动器,LMH0344 是自适应cable均衡器。

    不知道您具体应用是什么? 如果只是想延长电缆增强驱动能力,LMH0303就可以了。如果是想对长距离传输过来的信号进行均衡处理使用LMH0344.

    您可以看下这两款器件的典型应用: