This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB7340通讯问题求解



TUSB7340出现的问题

试用TUSB7340EVM连接,正常。仿照EVM新布板就会出现错误。

我们用USB3.0 U盘进行文件拷入拷出测试时,有时能拷贝文件,有时不能,且驱动快速不停打印如下信息:

xhci_hcd 0000:01:00.0: WARN: transfer error on endpoint usb 4-3: reset SuperSpeed USB device number 2 using xhci_hcd xhci_hcd 0000:01:00.0: WARN: short transfer on control ep xhci_hcd 0000:01:00.0: xHCI xhci_drop_endpoint called with disabled ep d6ab7120 xhci_hcd 0000:01:00.0: xHCI xhci_drop_endpoint called with disabled ep d6ab714c

跟踪transfer error on endpoint错误,发现是由USB3.0主控器回报的USB transaction error类型错误导致的,3.0规范写到USB transaction error可能由DPP error或者transaction timeout引起,USB 3.0规定,transaction timeout引起的USB transaction error,usb3.0主控器应halt相应ep,ep回应stall信息,主控器回报stall事件,从测试结果看,并没有监控到stall事件,而是不断复位设备。对主控器上电顺序涉及的信号进行了测量,符合上电顺序要求。

无法断定USB transaction error是由dpp error引起的,该如何解决?