Part Number: DS90UB954-Q1
Dear TI:
954的Mode pin硬件固定为同步模式,开机以后通过I2C修改寄存器搭配同步\非同步两种模式的953芯片,是否可以?
这样的话,954的硬件不需要改动,只需要下载不同的软件就可以搭配两种模式的953摄像头.
谢谢~~~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB954-Q1
Dear TI:
954的Mode pin硬件固定为同步模式,开机以后通过I2C修改寄存器搭配同步\非同步两种模式的953芯片,是否可以?
这样的话,954的硬件不需要改动,只需要下载不同的软件就可以搭配两种模式的953摄像头.
谢谢~~~
您好, 您的意思是即使我们使用MODE 引脚在硬件上配置sync mode,是否可以通过寄存器的修改改变成non-sync 模式是吗?
如果是这样的,是可以的,953的寄存器0x03的bit4配置为1,覆盖Strap pin MODE的配置。

需要注意的是953和954 要同时配置为sync或non-sync mode。
953是配置0x03. 954 需要配置寄存器0x58和0x6D。 0X58的bit[2:0]配置sync和non-sync的速率,0x6D的bit 1:0配置为00 CSI mode。