想请问一下,CDCE62005的时钟源,如果采用的是AUX_IN,单端的有源晶振,那么晶振频率必须在2MHz—42MHz之间吗?
另外Charge Pump的电流大小对输出有什么影响?
最后,如果VCO的频率不在1.75G—2.356G之间?输出会发生严重的偏移吗?
非常感谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
想请问一下,CDCE62005的时钟源,如果采用的是AUX_IN,单端的有源晶振,那么晶振频率必须在2MHz—42MHz之间吗?
另外Charge Pump的电流大小对输出有什么影响?
最后,如果VCO的频率不在1.75G—2.356G之间?输出会发生严重的偏移吗?
非常感谢!
对于CDCE62005来说,AUX_IN主要针对的是无源晶振crystal的输入频率范围为2MHz~42MHz。
charge pump能提供的电流很小,所以对输出基本上没什么影响。
使用有源晶振也是没问题的,但是CDCE62005内部已经有起振电路,所以可以直接接无源晶振。
Auxiliary Input is a single ended input including an on-board oscillator circuit so that a crystal may be connected.