This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HD3SS3212-Q1: 如果不专用于USB3.0,想应用于100M速率的通信的多路复用是否支持

Part Number: HD3SS3212-Q1
Other Parts Discussed in Thread: HD3SS3212

目前我的设计是一路100M和一路1.25G速率的通信,都是差分信号,共用一个外设接口。想通过程序控制具体哪路通信链路导通,是否可以选择HD3SS3212此芯片使用

  • HD3SS3212的-3dB 带宽能达到8GHz,所以100M和一路1.25G速率是没问题的。

    其次就是IO口的电压是否符合要求,1HD3SS3212的输入共模电压范围为0~2V,差分信号幅值能达到1800mV,如果电压也符合的话,使用HD3SS3212 可以满足您的应用。