Other Parts Discussed in Thread: DS25BR100
TI各位专家,你们好!
请教一下DS25BR101/110/150的芯片输出端内部也有一个端接电阻(如上图所示),请问一下这个输出端的内部端接通常是多大阻值?如果我在DS25BR101的后级采用DC耦合与receiver对接,那么receiver的输入端是否还需要100R端接电阻?
非常感谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
请问一下这个输出端的内部端接通常是多大阻值
首先您附上的这个图,输入输出端接的都是100ohm阻值。
另外您附上的这个图是针对DS25BR100/150的,DS25BR101的内部输入没有端接100ohm电阻。所以如果使用BR101,需要在靠近输入端外部端接100ohm。
如果我在DS25BR101的后级采用DC耦合与receiver对接,那么receiver的输入端是否还需要100R端接电阻?
需要,请参考数据手册P12关于OUTPUT INTERFACING的 介绍,其中Figure22 是BR100/101通过DC耦合和LVDS, CML或LVPECL接收器连接的应用。
Hello,Kailyn!非常感谢您的回复!我还有一点疑惑就是:既然DS25BR101芯片内部的输出端已经有100R端接的话,如果我在BR101后级的receiver差分输入端继续加100R端接,这种情况下,从原理上来说,receiver端的输入差分信号幅值不就减半了吗?从LVDS电气标准来看,这时候LVDS receiver端可能会因为LVDS幅值降低存在传输失败的风险。我的理解是:BR101内部已经有100R端接了,那么根据原理分析(对于3.5mA恒流源驱动而言),BR101后级的receiver的差分输入端应当是不用再接100R端接的。不确定这么理解是否正确,还希望您能继续解惑,再次感谢!祝好!
您好,通常都是在靠近接收端的位置端接终端匹配电阻。对于BR101/100/105这几款来说,主要是高速应用防止信号发生反射所以在输出端内部也端接了100ohm匹配电阻,为了和传输线的特征阻抗匹配。
关于您提到的幅值减半的理解,参考下面这个帖子:
您客气了,后续有什么问题,大家再讨论。