This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

接口论坛

Part Number: DS250DF230

同时使用3片DS250DF230:

第一片使用CPRI 9.8304Gbps或24.33.24Gbps,芯片CAL_CLK_IN接30.72MHz时钟

第二片使用25Gbps,CAL_CLK_IN接25MHz时钟

第三片使用10.3125Gbps,CAL_CLK_IN接25MHz时钟

使用SMBUS配置,读写寄存器正常。

如何快速配置3片芯片,工作在相应的速率下?能提供一下对应的寄存器和需要写入寄存器的值吗?