请教一个问题,我现在需要将数字摄像头传输距离增加到5~10米左右(最多不超过12米),数字摄像头是8bit信号,VS,HS,PCLK,PCLK在40~70M范围内。请问TI有没有推荐的方案可用,有没有专门用于数字摄像头传输的lvds serdes方案。另外,在摄像头端,希望能直接接camera输出的数字信号,而不用再增加fpga或者cpld做时序或者控制信号的逻辑。也简单看了sn65lv1023/1224的资料,但是感觉这俩芯片并不是针对视频应用设计的。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请教一个问题,我现在需要将数字摄像头传输距离增加到5~10米左右(最多不超过12米),数字摄像头是8bit信号,VS,HS,PCLK,PCLK在40~70M范围内。请问TI有没有推荐的方案可用,有没有专门用于数字摄像头传输的lvds serdes方案。另外,在摄像头端,希望能直接接camera输出的数字信号,而不用再增加fpga或者cpld做时序或者控制信号的逻辑。也简单看了sn65lv1023/1224的资料,但是感觉这俩芯片并不是针对视频应用设计的。
Dylan推荐的905/906属于FPDlink II的产品,我推荐的925/926是属于FPD link III的产品,FPDlink II和FPDlink III的区别除了FPDlink III的速率高之外,还具有HDCP content protection(option)以及Adaptive equalization 的特点。
了解了,谢谢。最后再问一下,这里905/906、925/926这两种方案,芯片价格都在7~8.5USD左右,请问有没有芯片价格在3~4USD以内的方案可以推荐。
您好,大概需求是 8bit数据+vs+hs,pclk能支持到70M。不一定非得24bit或者18bit的,传输距离最多5~12米,不超过12米。价格3~4USD之内,能直接支持带同步信号的数字视频格式,中间无需加fpga做逻辑转换。至于带不带均衡器,不是很理解,因为我也不太懂lvds,就想有现成的方案直接可以用起来,带与不带均衡器有什么区别啊?
看了下这类器件,价格和频率都满足的还不太好找,一般的支持到65Mhz, 像DS90CF383B&DS90CF384. 价格符合你的要求。 或者DS90C387R&DS90CF388这对,传输距离为5~15m,但价格又稍微贵了些。
kailyn,谢谢你的回复,我大概了解了,按您的说法,65M是一个坎,大部分的器件都支持到65M,超过65M的可能成本就贵很多了。但是您给我的两组器件都是需要多对lvds输出的。我再请想询问一下,如果改一下需求: 8bit数据+vs+hs,pclk能支持到65M,传输距离不超过12米,价格3~4USD之内,能直接支持带同步信号的数字视频格式,中间无需加fpga做逻辑转换,输出要求是1组lvds信号(而不是多对lvds)。这样的话,有合适的推荐型号么,再次麻烦了,不好意思。
你好, 给你推荐一个型号THCV231/236, 是纯硬件数字接口芯片,可以传输12米,比较符合你的要求,
你好,给你推荐一个比较符合你要求的高速率传输芯片 THCV231/236
THCV231可以将最高12Bit/pixel的LVCMOS并行信号转换为串行图像信号的发送端IC。最其具备大传输速率3.2Gbps的CML串行输出,可以将1080p60Hz的12bit摄像头图像信号通过一对双绞线或者一根同轴电缆进行传输。此外,可以通过双向的传输通道进行I2C信号传输。
THCV236/可以将THCV发送端IC输出的串行图像信号转换为最高32bit/pixel的LVCMOS并行图像信号的接受端IC。1080p60Hz的16bit的摄像头图像信号通过一对双绞线或者一根同轴电缆进行接收。此外,还具备一条可以用来传输I2C、UART或GPIO等串行信号的Sub-Link,向传输通道“Sub-Link" I2C/UART/GPIO(最高4条)
详细信息可看官网http://www.thine.co.jp/zh_cn/products/num_details/THCV231.html,我司可提供规格书、样片和技术支持,欢迎联系qq:2817821256 手机18682112448
您好,我是在校学生,目前实验室买了一个lvds的摄像头,我在调试板子的解串器I2C的时候,设定了slave id,但是用示波器测摄像头的输出发现没有波形,请问您遇到过这种问题吗?除了I2C还有需要调的东西吗?或者I2C我还有的东西没有调呀,麻烦您了,谢谢