Part Number: DS90UB921-Q1
DS90UB921TRHSRQ1我们目前用的720p 60fps,请问下ti921可以支持1920x1080 60fps么?或者支持1920x1080 30fps么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB921-Q1
DS90UB921TRHSRQ1我们目前用的720p 60fps,请问下ti921可以支持1920x1080 60fps么?或者支持1920x1080 30fps么?
您好,DS90UB921最大支持的像素时钟为96Mhz,1920x1080 60fps需要148.5MHz的像素时钟 ,所以不能支持1920x1080 60fps分辨率。
1920x1080 30fps相当于需要74.25Mhz的像素时钟,而921能支持到96Mhz,所以921能支持1920x1080 30fps分辨率。
需要像素时钟如何计算的,谢谢
Total data rate = [# active horizontal pixels + horizontal blanking] x [# active vertical lines + vertical blanking] x [frame rate] x [# bits/pixel]
以1920x1080 60fps为例,通常消隐时间大概为15%~25%范围,以15% 消隐计算的话,
像素时钟pixel clock=1920*1080*(1+15%)*60=143Mhz。
如果是24bit data的话 ,则total data rate=Pixel clock*24
ti921的1080p 30fps的寄存器配置需要你们提供下
921是不需要对分辨率进行配置的,只是给出了能支持的最大像素时钟,也就是说一定分辨率的视频源信号给921,921是可以支持的。